Table of contents 

Lubrication

  • Basic principles
  • Grease lubrication
  • Oil lubrication
  • Lubricating greases
  • Arcanol rolling bearing greases

Lubrication

Basic principles

Lubrication and maintenance are important for the reliable operation and long operating life of rolling bearings.

Functions of the lubricant

The lubricant should:

  • form a lubricant film on the contact surfaces that is sufficiently capable of supporting loads and thus preventing wear and premature fatigue
  • dissipate heat in the case of oil lubrication
  • give additional sealing of the bearing, in the case of grease lubrication, against the entry of both solid and fluid contaminants
  • dampen running noise
  • give protection against corrosion

Selection of the type of lubrication

Oil or grease lubrication

It should be determined as early as possible in the design process whether bearings should be lubricated using grease or oil.

The following factors are decisive in determining the type of lubrication and quantity of lubricant:

  • the operating conditions
  • the type and size of the bearing
  • the adjacent construction
  • the lubricant feed

Grease lubrication

Criteria for grease lubrication

In the case of grease lubrication, the following criteria must be considered:

  • very little design work required
  • the sealing action
  • the reservoir effect
  • long operating life with little maintenance work (lifetime lubrication possible in certain circumstances)
  • if relubrication is required, it may be necessary to provide collection areas for old grease and feed ducts
  • no heat dissipation by the lubricant
  • no rinsing out of wear debris and other particles

Oil lubrication

Criteria for oil lubrication

In the case of oil lubrication, the following criteria must be considered:

  • good lubricant distribution and supply to contact areas
  • dissipation of heat possible from the bearing (significant principally at high speeds and/or loads)
  • rinsing out of wear debris
  • very low friction losses with minimal quantity lubrication
  • more work required on feed and sealing

Under extreme operating conditions (such as very high temperatures, vacuum, aggressive media), it may be possible to use special lubrication methods such as solid lubricants in consultation with Schaeffler.

Design of lubricant feeds

Observe guidelines

The feed lines and lubrication holes in the housings and shafts ➤ Figure and ➤ Figure.

  • should lead directly to the lubrication hole in the rolling bearing
  • should be as short as possible

A separate feed must be provided for each bearing. Ensure that the feed lines are filled ➤ Figure; the feed line should be bled if necessary. Follow the instructions provided by the lubrication device manufacturer.

Lubricant feed lines

Arrangement of feed lines to more than one bearing on a shaft

Further information

Comprehensive information on the lubrication of rolling bearings is contained in Technical Product Information TPI 176. This publication can be requested from Schaeffler.

Grease lubrication

Greases can be differentiated in terms of their thickeners of varying composition and base oils. The base oils of greases are covered by the information in the section Oil lubrication ➤ link.

Composition of a grease

Conventional greases have metal soaps as thickeners and a mineral base oil ➤ Figure. They also contain additives. These have a specific influence on, for example, the characteristics in relation to wear prevention, corrosion prevention or resistance to ageing. These combinations of additives are not, however, fully effective across every temperature and load range.

Greases exhibit widely varying behaviour in response to environmental influences such as temperature and moisture.

Type of grease


Thickener


Additives


Base oil


Grease

Lubricants must always be checked for their compatibility with:

  • other lubricants
  • anti-corrosion agents
  • thermoplastics, thermosets and elastomers
  • light and non-ferrous metals
  • coatings
  • colouring agents and paints
  • and the environment. When considering compatibility with the environment, attention must be paid to toxicity, biodegradability and water pollution class

Type of grease

The characteristics of a grease are dependent on:

  • the base oil
  • the viscosity of the base oil (this is significant for the speed range)
  • the thickener (the shear strength is significant for the speed range)
  • the additives

Consistency of greases

Greases are subdivided into consistency classes (NLGI classes to DIN 51818). For rolling bearings, classes 1, 2, 3 should be used in preference ➤ Figure.

Consistency of greases

NLGI classes

Selection of suitable grease

The grease is determined by the operating conditions

Rolling bearing greases K to DIN 51825 are suitable.

Greases should be selected in accordance with the operating conditions of the bearing:

  • temperature
  • pressure conditions ➤ link
  • speed ➤ link
  • water and moisture ➤ link

Operating temperature range

The grease must correspond to the operating temperatures

The operating temperature range of the grease must correspond to the range of possible operating temperatures in the rolling bearing.

Grease manufacturers indicate an operating temperature range for their rolling bearing greases K to DIN 51825.

The upper value is determined in accordance with DIN 51821 by means of testing on the FAG rolling bearing grease test rig FE9. At the upper operating temperature, a 50% failure probability rate (F50) of at least 100 hours must be achieved in this test.

The lower value is defined in accordance with DIN 51825 by means of flow pressure. The flow pressure of a grease is the pressure required to press a stream of grease through a defined nozzle. For greases of type K, the flow pressure at the lower operating temperature must be less than 1 400 mbar.

The use of flow pressure in determining the lower operating temperature only indicates, however, whether the grease can be moved at this temperature. This cannot be used to give an indication of its suitability for use in rolling bearings at low temperatures.

In addition to the lower operating temperature of a grease, therefore, the low temperature frictional torque is also determined in accordance with ASTM D 1478or IP 186/93. At the lower operating temperature, the starting torque must not exceed 1 000 Nmm and the running torque must not exceed 100 Nmm.

Schaeffler recommends that greases should be used in accordance with the bearing temperature normally occurring in the standard operating range, in order to achieve a reliable lubricating action and an acceptable grease operating life ➤ Figure.

At low temperatures, greases release very little base oil. This can result in lubricant starvation. Schaeffler therefore recommends that greases are not used below the lower continuous limit temperature ϑlower limit on a permanent basis ➤ Figure. This is approx. 20 K above the lower operating temperature of the grease as stated by the grease manufacturer.

The upper continuous limit temperature ϑupper limit must not be exceeded if a temperature-induced reduction in the grease operating life is to be avoided; see Grease operating life ➤ link.

At consistently low temperatures (for example in cold store applications), it must be ensured that the grease releases sufficient oil in relation to the bearing type.

Operating temperature range

ϑ = operating temperature

ΔT = temperature difference


Upper operating temperature according to grease manufacturer


ϑupper limit


ϑlower limit


Lower operating temperature according to grease manufacturer


Standard operating range

Pressure properties

The pressure properties are dependent on the viscosity

The viscosity at operating temperature must be sufficiently high for the formation of a lubricant film capable of supporting loads. At high loads, greases with EP characteristics (“extreme pressure”) and high base oil viscosity should be used (KP grease to DIN 51825). Such greases should also be used for bearings with substantial sliding or line contact.

Silicone greases should only be used at low loads (P ≦ 0,03 · C).

Greases with solid lubricants should preferably be used for applications with mixed or boundary friction conditions. The solid lubricant particle size must not exceed 5 μm.

Speed

Speed parameter n · dM is a criterion for grease selection

Greases should be selected in accordance with the speed parameter n · dM for grease ➤ Table:

  • For rolling bearings running at high speeds or with a low starting torque, greases with a high speed parameter should be used
  • For bearings running at low speeds, greases with a low speed parameter should be used

Under centrifugal accelerations > 500 · g, separation (of the thickener and base oil) may occur. In this case, please consult the lubricant manufacturer.

The consistency of polycarbamide greases can be altered by shear stresses to a greater extent than that of metal soap greases.

Water and moisture

Water reduces the operating life

Water in the grease has a highly detrimental effect on the operating life of bearings:

  • the static behaviour of greases in the presence of water is assessed in accordance with DIN 51807 ➤ Figure
  • the anti-corrosion characteristics can be tested according to DIN 51802 (Emcor test) – information is given in the grease manufacturer’s data sheets

Behaviour in the presence of water in accordance with DIN 51807


Blank


Grease sample


Glass slide

Grease operating life

The grease operating life tfG applies where this is below the calculated bearing life and the bearings are not lubricated.

A guide value can be determined in approximate terms in accordance with ➤ Equation:

Guide value for grease operating life

Legend

tfG h

Guide value for grease operating life

tf h

Basic grease operating life

KT, KP,
KR, KU
-

Correction factors for temperature, load, oscillation and environment

If a grease operating life > 3 years is required, this must be agreed in consultation with the lubricant manufacturer.

Guidelines on calculating the grease operating life ➤ link.

Basic grease operating life

This applies under the preconditions according to ➤ Table.

Preconditions for the basic grease operating life

Precondition

Bearing temperature

< upper continuous limit temperature ϑupper limit

Load ratio

C0/P = 20

Speed and load

Constant

Load in main direction

Radial in radial bearings, axial in axial bearings

Axis of rotation

Horizontal for radial bearings

Inner ring

Rotating

Environmental influences

No disruptive influences

The basic grease operating life tf is dependent on the bearing-specific speed parameter kf · n · dM and is calculated using ➤ Figure.

Legend

kf -

Bearing type factor ➤ Table

n min–1

Operating speed or equivalent speed

dM mm

Mean bearing diameter (d + D)/2

Calculation of basic grease operating life

Calculation of basic grease operating life

tf = basic grease operating life

kf · n · dM = bearing-specific speed parameter


Factor kf – as a function of bearing type

Bearing type

Factor

kf

Deep groove ball bearings, single row, Generation C

0,8

Deep groove ball bearings, single row

1

Deep groove ball bearings, double row

1,5

Angular contact ball bearings, single row

1,6

Angular contact ball bearings, single row, X-life

1,3

Angular contact ball bearings, double row

2

Angular contact ball bearings, double row, X-life

1,6

Spindle bearings, α = 15°

0,75

Spindle bearings, α = 25°

0,9

Four point contact bearings

1,6

Four point contact bearings, X-life

1,3

Self-aligning ball bearings

1,45

Axial deep groove ball bearings

5,5

Axial angular contact ball bearings, single row

1,8

Axial angular contact ball bearings, double row

2

Cylindrical roller bearings, single row

2

Cylindrical roller bearings LSL, ZSL

3

Cylindrical roller bearings, double row

3

Cylindrical roller bearings, full complement

6

Tapered roller bearings

4

Spherical roller bearings

8

Toroidal roller bearings TORB

8

Needle roller and cage assemblies, needle roller bearings

3,6

Drawn cup needle roller bearings

4,2

Yoke type track rollers, stud type track rollers with cage, stud type track rollers with full complement cylindrical roller set

20

Yoke type track rollers, stud type track rollers,
full complement needle roller set

40

Ball bearing type track rollers, single row

1

Ball bearing type track rollers, double row

2

Yoke type track rollers PWTR, stud type track rollers PWKR

6

Crossed roller bearings

4,4

Axial needle roller bearings, axial cylindrical roller bearings

58

Radial insert ball bearings, housing units

1

Guidelines on calculating the grease operating life

Combined rolling bearings

The radial and axial bearing components must be calculated separately; the decisive value is the shorter grease operating life.

Rotating outer ring

If the outer ring rotates, there may be a reduction in the grease operating life.

In the case of yoke and stud type track rollers:

  • the angular misalignment must be zero
  • the effect of the rotating outer ring on the grease operating life is taken into consideration in the bearing type factor kf

Restrictions of the calculation

The grease operating life cannot be determined using the method described in the following cases:

  • if the grease can leave the bearing arrangement
    • there is excessive evaporation of the base oil
    • in bearing positions without seals
    • in axial bearings with a horizontal axis of rotation
  • if air is sucked into the rolling bearing during operation
    • this can cause the grease to oxidise
  • for bearing arrangements that have a vertical shaft
  • in combined rotary and linear motion (the grease is distributed over the whole stroke length)
  • if contamination, water or other fluids enter the bearing
  • for spindle bearings
  • for drawn cup roller clutches
  • for screw drive bearings
  • for high precision bearings for combined loads
  • for super precision cylindrical roller bearings NN30

The additional guidelines on lubrication in the product chapters must be observed.

Correction factors for determining the grease operating life

Temperature factor KT

If the bearing temperature is higher than the reference temperature ϑreference, KT must be determined from the diagram ➤ Figure.

The diagram must not be used if the bearing temperature is higher than the upper operating temperature of the grease used ➤ Table. If necessary, a different grease must be selected or contact must be made with Schaeffler.

Depending on the grease quality, temperature factors KT > 1 are also possible below the reference temperature.

Temperature factor

KT = temperature factor


K above ϑreference

Load factor KP

The factor KP is dependent on the bearing and describes the reduction at higher load (this places greater strain on the grease) ➤ Figure and ➤ Table.

Load correction factor Kp

Kp = load correction factor

C0/P = ratio between basic static load rating and equivalent dynamic bearing load

See:





in ➤ Table

Correction factor for load KP

Curve
➤ Figure

Bearing type

Axial angular contact ball bearings, double row

Axial deep groove ball bearings
Axial needle roller bearings, axial cylindrical roller bearings

Crossed roller bearings

Spherical roller bearings with central rib

Needle roller and cage assemblies, needle roller bearings

Drawn cup needle roller bearings

Cylindrical roller bearings, double row (excluding NN30)
Yoke type track rollers PWTR, stud type track rollers PWKR

Yoke and stud type track rollers with cage, full complement cylindrical roller set

Yoke and stud type track rollers, full complement needle roller set

Four point contact bearings

Cylindrical roller bearings LSL, ZSL

Cylindrical roller bearings, full complement

Cylindrical roller bearings, single row (constant or alternating load)

Tapered roller bearings

Barrel roller bearings

Spherical roller bearings without central rib (E1)

Toroidal roller bearings

Deep groove ball bearings (single or double row)
Angular contact ball bearings (single or double row)

Self-aligning ball bearings

Ball bearing track rollers (single or double row)

Radial insert ball bearings, housing units

Oscillation factor KR

The factor KR applies for an angle of oscillation φ < 180° ➤ Figure. Oscillating motion places a greater strain on the grease than does rotating motion.

In order to reduce fretting corrosion, the lubrication interval should be reduced.

If the rolling elements do not undergo complete rotation, please consult Schaeffler.

Correction factor for oscillation KR

KR = correction factor for oscillation

φ = angle of oscillation


Angle of oscillation φ < 5°requires special lubricants

Environmental factor KU

The factor KU takes account of the influences of moisture, shaking forces, slight vibration (leading to fretting corrosion) and shocks ➤ Table. It does not take account of extreme environmental influences such as water, aggressive media, contamination, radiation and extreme vibrations such as those occurring in vibratory machines.

In relation to contamination, the influence of contamination on rating life calculation must also be noted.

Environment factor KU

Environmental influence

Factor

KU

Slight (e. g. test rig)

1

Moderate (standard)

0,8

Heavy (e. g. outdoor application)

0,5

Relubrication intervals

Observe lubrication intervals

Where rolling bearings are relubricated, attention must be paid to the lubrication interval in order to ensure reliable function of the bearings.

The precise lubrication interval should be determined by tests conducted under application conditions. To do this:

  • sufficiently long observation periods must be used
  • the condition of the grease must be checked at regular intervals

For reasons of operational reliability, relubrication intervals of > 1 year are not recommended.

Lubrication interval guide value

Experience shows that the guide value for most applications is ➤ Equation.

Guide value for relubrication interval

Legend

tfR h

Guide value for relubrication interval

tfG h

Guide value for grease operating life


Relubrication conditions

The grease used for relubrication must be the same as that used in initial greasing. If other greases are used, the miscibility and compatibility of the greases must be checked.

Relubrication quantity

Due to the compact construction of the bearings, relubrication should be carried out using 50% to 80% of the initial greasing quantity (recommendation).

If feed lines filled with air are present, the filling volume of the feed lines should be included in calculation of the relubrication quantity.

Relubrication

Relubrication should always be carried out as follows:

  • with the bearing still warm from operation and rotating if safe to do so
  • before the bearing comes to rest if safe to do so
  • before extended breaks in operation

Relubrication should continue until a fresh collar of grease appears at the seal gaps. Old grease must be allowed to leave the bearing unhindered.

Grease reservoir

The initial greasing quantity is between 30% and 100% of the available volume in the bearing, dependent on the bearing type and operating conditions.

A grease reservoir can extend the grease operating life. The grease in the reservoir must be in constant contact with the grease on the raceway. The grease operating life does not increase proportionally with the size of the grease reservoir.

The volume of the grease reservoir should correspond to the volume in the bearing between the inner and outer ring (not taking account of the cage and rolling elements) ➤ Figure and ➤ Figure.

Evaporation of the base oil should be prevented by design measures, for example by sealing shields ➤ Figure and ➤ Figure.

Grease reservoir on one side

Sealing washer

Grease reservoir

Grease reservoir on both sides

Sealing washer

Grease reservoir

Miscibility

Preconditions

Mixtures of greases should be avoided if at all possible. If they are unavoidable, the following preconditions must be fulfilled:

  • The base oil must be the same
  • The thickener types must match
  • The base oil viscosities must be similar (they must not differ by more than one ISO VG class )
  • The consistency must be identical (NLGI class)

Miscibility of greases must always be agreed in consultation with the lubricant manufacturer.

Even when these preconditions are fulfilled, impairment of the performance capability of the mixed grease cannot be ruled out.

If a decision is taken to change to a different grease grade, the grease should be rinsed out if this is possible. Further relubrication should be carried out after a shortened period.

If incompatible greases are mixed, this can lead to considerable structural changes. Substantial softening of the grease mixture may also occur. Definite statements on miscibility can only be obtained by means of suitable tests.

Storage life

In general, the greases can be stored for 3 years.

Preconditions

The preconditions are:

  • a closed room or store
  • temperatures between 0 °C and +40 °C
  • relative humidity no more than 65%
  • no influence of chemical agents (vapours, gases, fluids)
  • the rolling bearings are sealed

Lubricants age due to environmental influences. The information provided by lubricant manufacturers must always be observed.

After long periods of storage, the start-up frictional torque of greased bearings can be temporarily higher than normal. The lubricity of the grease may also have deteriorated.

Since the lubrication characteristics of greases vary and different raw materials may be used for greases of the same name, Schaeffler cannot offer any guarantees either for the lubricants used by customers for relubrication or for their characteristics.

Oil lubrication

Mineral oils or synthetic oils are suitable

For the lubrication of rolling bearings, mineral oils and synthetic oils are essentially suitable. Oils with a mineral oil base are used most frequently. They must, as a minimum, fulfil the requirements in accordance with DIN 51517 or DIN 51524.

Special oils, often synthetic oils, are used under extreme operating conditions or where there are special requirements relating to oil resistance. In these cases, please consult the lubricant manufacturers or Schaeffler.

Operating temperatures

The information provided by the lubricant manufacturer should be taken as authoritative.

Selection of suitable oil

The achievable bearing life and security against wear are higher with better separation of the contact surfaces by a lubricant film ➤ Figure.

Lubricant film in the contact zones

hmin = minimum lubricant film thickness


Entry zone


Pressure curve according to EHD theory


Exit zone


Lubricant

Reference viscosity for mineral oils

Guide value for ν1

The guide value for ν1 is dependent on the mean bearing diameter dM and the speed n. It takes account of the EHD theory of lubricant film formation and practical experience.

Depending on the operating speed, the oil at operating temperature must have at least the reference viscosity ν1 ➤ Figure and ➤ Figure.

Calculating the reference viscosity ν1

ν1 = reference viscosity

dM = mean bearing diameter

n = speed

ν/ϑ diagram for mineral oils

ν = operating viscosity

ϑ = operating temperature

ν40 = viscosity at +40 °C

Calculation of reference viscosity

Determine ν1

The reference viscosity ν1 is calculated as follows:

  • Allocate ν1 to a nominal viscosity between ISO VG 10 and ISO VG 1500 (mid‑point viscosity in accordance with ISO 3448)
  • Round intermediate values to the nearest ISO VG (due to the steps between groups)

This method cannot be used for synthetic oils, since these have different V/P (viscosity/pressure) and V/T (viscosity/temperature) characteristics. In these cases, please consult Schaeffler.

Influence of temperature on viscosity

Aim for VI of 95

As the temperature increases, the viscosity of the oil decreases. This temperature-dependent change in the viscosity is described using the viscosity index VI. For mineral oils, the viscosity index should be at least 95.

When selecting the viscosity, the lower operating temperature must be taken into consideration, since the increasing viscosity will reduce the flowability of the lubricant. As a result, the level of power losses may increase.

Viscosity ratio κ

A very long life can be achieved with a viscosity ratio κ = ν/ν1 = 3 to 4 (ν = operating viscosity). Highly viscous oils do not, however, bring only advantages. In addition to the power losses arising from lubricant friction, there may be problems with the feed and removal of oil at low or even at normal temperatures.

Aim for long fatigue life

The oil selected must be sufficiently viscous that it gives the highest possible fatigue life. It must also be ensured that the bearings are always supplied with adequate quantities of oil.

Pressure properties and anti-wear additives

Oils with wear additives

If the bearings are subjected to high loads or if the operating viscosity ν is less than the reference viscosity ν1, oils with anti-wear additives (type P in accordance with DIN 51502) should be used. Such oils are also necessary for rolling bearings with a substantial proportion of sliding contact (for example, bearings with line contact). These additives form boundary layers to reduce the harmful effects of metallic contact occurring at various points (wear).

The suitability of these additives varies and is normally heavily dependent on temperature. Their effectiveness can only be assessed by means of testing in the rolling bearing (for example on our test rig FE8 to DIN 51819).

Silicone oils should only be used for low loads (P ≦ 0,03 · C).

Compatibility

Check compatibility prior to use

Before an oil is used, its behaviour must be checked in relation to plastics, seal materials (elastomers) and light and non-ferrous metals. This must always be checked under dynamic loading and at operating temperature.

Synthetic oils must always be checked for their compatibility. The lubricant manufacturer must be consulted on this at the same time.

Miscibility

Avoid mixing different oils

The mixing of different oils should be avoided wherever possible. In particular, the presence of different additive packages may lead to undesirable interactions.

In general, oils with a mineral oil base and the same classification are miscible, for example type HLP with type HLP. The viscosities should vary by no more than one ISO VG class.

Synthetic oils must always be checked for their compatibility. The lubricant manufacturer must be consulted on this at the same time.

Miscibility must be checked in advance for each individual case.

Cleanliness

An oil filter should be used

The cleanliness of the oil has a considerable influence on the rating life of the bearings. Schaeffler therefore recommends that an oil filter should be provided; attention must be paid to the filtration rate. The filter mesh should be < 25 μm.

Lubrication methods

Proven methods

The essential lubrication methods are:

  • drip feed oil lubrication
  • pneumatic oil lubrication (to protect the environment, this should be used as a substitute for oil mist lubrication)
  • oil bath lubrication (immersion or sump lubrication)
  • recirculating oil lubrication

Drip feed oil lubrication

This is suitable for bearings running at high speeds ➤ Figure. The oil quantity required is dependent on the type and size of bearing, the operating speed and the load. The guide value is between 3 drops/min and 50 drops/min for each rolling element raceway (one drop weighs approx. 0,025 g).

Excess oil must be allowed to flow out of the bearing arrangement.

Drip feed oil lubrication


Pneumatic oil lubrication

This method is particularly suitable for radial bearings running at high speeds and under low loads (n · dM = 800 000 to 3 000 000 min–1 · mm) ➤ Figure. Clean compressed air free from moisture feeds oil to the bearing. This generates an excess pressure, which prevents contaminants from entering the bearing.

With a pneumatic oil lubrication system designed for minimal quantity lubrication, low frictional torque and a low operating temperature can be achieved.

Parameters

Parameters for design of the lubrication system should be requested from the equipment manufacturers.

Pneumatic oil lubrication of axial bearings should be avoided if possible.

The oil quantity required for adequate supply is dependent on the bearing type.

Pneumatic oil lubrication has little cooling effect.

Follow the instructions provided by the manufacturers of the lubrication systems.

Pneumatic oil lubrication


To the pneumatic oil unit

Oil bath lubrication

The oil level should reach the centre line of the lowest rolling element ➤ Figure. If the oil level is higher than this, the bearing temperature may increase at high circumferential velocities (with losses due to splashing). Furthermore, foaming of the oil may occur.

n · dM values

In general, it is suitable for speeds up to n · dM = 300  000 min–1 · mm. At n · dM < 150  000 min–1 · mm, the bearing may be completely immersed.

In bearings with an asymmetrical cross-section, oil return ducts must be provided due to the pumping effect so that recirculation can be achieved.

Axial bearings

In axial bearings, the oil level must cover the inside diameter of the axial cage.

Proportion oil quantity adequately

The oil quantity in the housing must be adequately proportioned, as otherwise very short oil change intervals will be necessary.

Oil bath lubrication


Oil sump

Recirculating oil lubrication

In recirculating oil lubrication, the oil is subjected to additional cooling ➤ Figure. The oil can therefore dissipate heat from the bearing. The quantity of oil required for heat dissipation is dependent on the cooling conditions.

Recirculating oil lubrication


Filter


Pump


Cooling system

Oil quantity

The oil quantities are matched to the operating conditions ➤ Figure. The diagram indicates oil quantities that can be fed through the bearing without pressure with a side feed arrangement and banking up to the lower edge of the shaft.

Bearings with asymmetrical cross-section

For bearings with an asymmetrical cross-section (such as angular contact ball bearings, tapered roller bearings, axial spherical roller bearings), larger throughput quantities are permissible due to the pumping effect than for bearings with a symmetrical cross-section. Large quantities can be used to dissipate wear debris or heat.

Oil quantities

= oil quantity

D = outside bearing diameter

a = oil quantity sufficient for lubrication

b = upper limit for bearings of symmetrical design

c = upper limit for bearings of asymmetrical design
a1; b1; c1: D/d > 1,5
a2; b2; c2: D/d ≦ 1,5


Increasing oil quantity required for heat dissipation


No heat dissipation required

Design of adjacent construction for oil lubrication

The lubrication holes in the housing and shaft must align with those in the rolling bearings. Adequate cross-sections must be provided for annular slots, pockets, etc. The oil must be able to flow out without pressure (this prevents oil build-up and additional heating of the oil).

Axial bearings

In axial bearings, the oil must always be fed from the inside to the outside.

Guide values

The cross-section of the oil outlet hole should be significantly larger than that of the inlet ➤ Figure.

The cross-section Arab is dependent on the oil quantity and the viscosity ➤ Equation.

Outlet cross section

Legend

Arab mm2

Outlet cross-section taking account of viscosity

Kab -

Correction factor for viscosity ➤ Table

Aab mm2

Outlet cross-section ➤ Figure

Outlet cross-section (guide values)

Aab = cross-section for pressure-free oil runout

= oil quantity


Correction factor Kab

Viscosity

Factor

ν

Kab

mm2/s

from

to

from

to

‒

30

1

‒

30

60

1,2

1,6

60

90

1,8

2,2

90

120

2,4

2,8

120

150

3

3,4

Oil injection lubrication

Advantages and disadvantages

In bearings running at high speeds, the oil is injected into the gap between the cage and bearing ring ➤ Figure. Injection lubrication using large recirculation quantities is associated with high power loss.

Heating of the bearings can only be held within limits with a considerable amount of effort. The appropriate upper limit for the speed parameter n · dM = 1 000 000 min-1 · mm for recirculating lubrication with suitable bearings (for example spindle bearings) can be exceeded to a considerable degree when using injection lubrication.

Oil injection lubrication


Angular contact ball bearing


Tapered roller bearing


Oil outlet holes

Heat dissipation by the lubricant

Values L and L can be calculated

Oil can dissipate frictional heat from the bearing. It is possible to calculate the heat flow L that is dissipated with the lubricant and the necessary lubricant volume flow L.

Heat flow

The total dissipated heat flow due to possible heating by an external source can be calculated using ➤ Equation, while the heat flow dissipated by the lubricant can be calculated using ➤ Equation.

Total dissipated heat flow

Heat flow dissipated by the lubricant

Legend

kW

Total dissipated heat flow

n min-1

Operating speed or equivalent speed

M0 Nmm

Frictional torque as a function of speed

M1 Nmm

Frictional torque as a function of load

E kW

Heat flow due to heating by external source

L kW

Heat flow dissipated by the lubricant

S kW

Heat flow dissipated via the bearing seating surfaces


Lubricant volume flow

The lubricant volume flow can be calculated approximately ➤ Equation.

Lubricant volume flow

Legend

L


l/min


Lubricant volume flow

L kW

Heat flow dissipated by the lubricant

ΔϑL K

Difference between oil inlet temperature and oil outlet temperature


Guide values

If these values cannot be calculated, the guide values according to ➤ Figure apply for the temperature difference of ΔϑL = 10 K.

Guide values for the oil quantity in cooling and lubrication

NR = frictional power

= oil quantity


No account is taken of thermal conduction, radiation or convection


Empirical values for normal cooling conditions


Empirical values for very good cooling conditions

Oil changes

One oil change per year is usually sufficient

At temperatures in the bearing of less than +50 °C and with only slight contamination, an oil change once per year is generally sufficient. Guide values for oil change intervals are given in ➤ Figure. The precise oil change intervals should be agreed in consultation with the oil manufacturer.

Severe operating conditions

Under severe conditions, the oil should be changed more frequently. This applies, for example, in the case of higher temperatures and low oil quantities with a high circulation index. The circulation index indicates how often the entire oil volume available is recirculated or pumped per hour ➤ Equation.

Circulation index

Oil change intervals

ϑ = oil sump temperature

t = oil change interval


Synthetic gearbox oils


Mineral gearbox oils

Lubricating greases

Greases

Designation3)

Classification

Type of grease

Operating temperature range

Upper continuous limit temperature

ϑupper limit1)

Designation

NLGI class

Speed parameter

n · dM

ISO VG class (base oil)2)

Designation3)

Recommended Arcanol grease for relubrication

°C

°C

min-1 · mm

from

to

from

to

from

to

GA01

Ball bearing grease for ϑ < +180 °C

Polycarbamide

Ester oil

–30

+180

+125

GA01

2

3

600  000

 68

220

GA01

‒

GA02

Ball bearing grease for ϑ < +160 °C

Polycarbamide

SHC

–40

+160

+90

GA02

2

3

500  000

 68

220

GA02

‒

GA13

Standard ball bearing and insert bearing grease for D > 62 mm

Lithium soap

Mineral oil

–20

+120

+75

GA13

3

‒

500  000

 68

150

GA13

Multi2

GA14

Low-noise ball bearing grease for D ≦62 mm

Lithium soap

Mineral oil

–30

+120

+75

GA14

2

‒

500  000

 68

150

GA14

Multi2

GA15

Low-noise ball bearing grease for high speeds

Lithium soap

Ester oil/SHC

–40

+120

+75

GA15

2

3

1  000  000

 22

 32

GA15

‒

GA22

Free-running grease with low frictional torque

Lithium soap

Ester oil, mineral oil

–50

+120

+70

GA22

2

‒

1  500  000

 10

  22

GA22

‒

L069

Insert bearing grease for wide temperature range

Polycarbamide

Ester oil

–40

+180

+120

L069

2

‒

700  000

 68

220

L069

‒

GA08

Grease for line contact

Lithium complex soap

Mineral oil

–20

+140

+95

GA08

2

3

500  000

150

320

GA08

Load150

GA26

Standard grease for drawn cup roller clutches

Calcium/lithium soap

Mineral oil

–20

+80

+60

GA26

2

‒

500  000

 10

 22

GA26

‒

GA28

Screw drive bearing grease

Lithium soap

Synthetic oil/mineral oil

–30

+140

+80

GA28

2

‒

800  000

 15

 100

GA28

Multitop

GA11

Rolling bearing grease resistant to media for temperatures up to +250 °C

PTFE

Alkoxyfluoroether

–30

+260

+200

GA11

2

‒

300  000

460

680

GA11

Temp200

GA47

Rolling bearing grease resistant to media for temperatures up to +140 °C

Barium complex soap

Mineral oil

–20

+130

+70

GA47

1

2

350  000

150

320

GA47

‒

  1. The upper continuous limit temperature ϑupperlimit must not be exceeded if a reduction in the grease operating life due to temperature is to be avoided.
  2. Dependent on bearing type.
  3. GA.. Stands for Grease Application Group.., based on Grease Spec 00.

Arcanol rolling bearing greases

Arcanol rolling bearing greases

Grease

+++ = extremely suitable
++  = highly suitable
+  = suitable
–  = less suitable
––   = not suitable

Characteristic applications

Operating temperature

Continuous limit
temperature

Thickener

Base oil

Grease

Consistency

Base oil viscosity at +40 °C

Temperatures

Low friction, high speed

High load, low speed

Vibrations

Support for seals

Relubrication facility

Grease

°C

°C

NLGI

mm2/s

from

to

Low

High

Multi-purpose greases

Multitop

  • Ball and roller bearings in rolling mills
  • Construction machinery
  • Spinning and grinding spindles
  • Automotive engineering

–501)

+140

+80

Lithium soap

Partially synthetic oil

Multitop

2

82

+++

++

++

+++

++

+

+++

Multitop

Multi-purpose greases

Multi2

  • Ball bearings up to D ≦ 62 mm in electric motors
  • Agricultural and construction machinery
  • Household appliances

–30

+120

+75

Lithium soap

Mineral oil

Multi2

2

110

++

+

+

+

+

+

+++

Multi2

Multi-purpose greases

Multi3

  • Ball bearings from D > 62 mm in electric motors
  • Agricultural and construction machinery
  • Fans

–30

+120

+75

Lithium soap

Mineral oil

Multi3

3

80

++

+

+

+

++

++

++

Multi3

Grease

Characteristic applications

Operating temperature

Continuous limit
temperature

Thickener

Base oil

Grease

Consistency

Base oil viscosity at +40 °C

Temperatures

Low friction, high speed

High load, low speed

Vibrations

Support for seals

Relubrication facility

Grease

°C

°C

NLGI

mm2/s

from

to

Low

High

High loads

Load150

  • Ball, roller and needle roller bearings
  • Linear guidance systems in machine tools

–20

+140

+95

Lithium complex soap

Mineral oil

Load150

2

160

+

++

–

+++

++

++

++

Load150

High loads

Load220

  • Ball and roller bearings in rolling mill plant
  • Paper machinery
  • Rail vehicles

–20

+140

+80

Lithium/calcium soap

Mineral oil

Load220

2

245

+

+

–

+++

++

++

++

Load220

High loads

Load400

  • Ball/roller bearings in mining machinery
  • Construction machinery
  • Wind turbine main bearings

–401)

+130

+80

Lithium/calcium soap

Mineral oil

Load400

2

400

+

+

–

+++

++

++

++

Load400

High loads

Load460

  • Ball/roller bearings
  • Wind turbines
  • Bearings with pin cage

–401)

+130

+80

Lithium/calcium soap

Mineral oil

Load460

1

400

++

+

–

+++

++

–

++

Load460

High loads

Load1000

  • Ball/roller bearings in mining machinery
  • Construction machinery
  • Cement plant

–301)

+130

+80

Lithium/calcium soap

Mineral oil

Load1000

2

1  000

+

+

––

+++

++

++

++

Load1000

Grease

Characteristic applications

Operating temperature

Continuous limit
temperature

Thickener

Base oil

Grease

Consistency

Base oil viscosity at +40 °C

Temperatures

Low friction, high speed

High load, low speed

Vibrations

Support for seals

Relubrication facility

Grease

°C

°C

NLGI

mm2/s

from

to

Low

High

High temperatures

Temp90

  • Ball and roller bearings in couplings
  • Electric motors
  • Automotive engineering

–40

+160

+90

Polycarbamide

Partially synthetic oil

Temp90

3

148

+++

++

+

+

+

++

++

Temp90

High temperatures

Temp110

  • Ball and roller bearings in electric motors
  • Automotive engineering

–35

+160

+110

Lithium complex soap

Partially synthetic oil

Temp110

2

130

+++

+++

++

+

+

+

+

Temp110

High temperatures

Temp120

  • Ball and roller bearings in continuous casting plant
  • Paper machinery

–30

+180

+120

Polycarbamide

Alkoxyfluoro oil

Temp120

2

400

++

+++

–

+++

+

++

+

Temp120

High temperatures

Temp200

  • Ball and roller bearings in guide rollers for baking machinery
  • Kiln trucks and chemical plant
  • Piston pins in compressors

–30

+260

+200

PTFE

Fluoridated polyether oil

Temp200

2

550

++

+++

––

++

+

+

+

Temp200

Special requirements

Speed2.6

  • Ball bearings in machine tools
  • Spindle bearings
  • Rotary table bearings
  • Instrument bearings

–40

+120

+80

Lithium complex soap

Synthetic oil

Speed2.6

2 – 3

25

+++

+

+++

––

–

+

+

Speed2.6

Special requirements

Vib3

  • Ball and roller bearings in rotors for wind turbines (blade adjustment)
  • Packaging machinery
  • Rail vehicles

–30

+150

+90

Lithium complex soap

Mineral oil

Vib3

3

170

++

++

–

++

+++

++

–

Vib3

Special requirements

FOOD2

  • Ball and roller bearings in applications with food contact (NSF-H1 registration, kosher and halal certification)

–30

+120

+70

Aluminium complex soap

Synthetic oil

FOOD2

2

150

++

–

+

+

+

+

+++

FOOD2

Special requirements

CLEAN M

  • Ball, roller and needle roller bearings as well as linear guidance systems in clean room applications

–30

+180

+90

Polycarbamide

Ester

CLEAN M

2

103

+++

+++

+

+

+

+

++

CLEAN M

Special requirements

Motion2

  • Ball and roller bearings in oscillating operation
  • Slewing rings in wind turbines

–40

+130

+75

Lithium soap

Synthetic oil

Motion2

2

50

+++

+

–

++

+++

++

+

Motion2

Grease

Characteristic applications

Operating temperature

Continuous limit
temperature

Thickener

Base oil

Grease

Consistency

Base oil viscosity at +40 °C

Temperatures

Low friction, high speed

High load, low speed

Vibrations

Support for seals

Relubrication facility

Grease

°C

°C

NLGI

mm2/s

from

to

Low

High

  1. Measurement values according to Schaeffler FE8 low temperature test.
Available containers ➤ Table

Available containers

Grease container sizes

Arcanol grease1)

Tube

Cartridge

Can

Bucket

Hobbock

Drum

70 g

250 g

400 g

1 kg

5 kg

12,5 kg

25 kg

50 kg

180 kg

Multitop

‒

●

●

●

●

●

●

‒

●

Multi2

‒

●

●

●

●

●

●

‒

●

Multi2

‒

●

●

●

●

●

‒

‒

●

Load150

‒

‒

●

●

‒

●

‒

●

‒

Load220

‒

‒

●

●

‒

●

●

‒

●

Load400

‒

‒

●

●

●

●

●

●

●

Load460

‒

‒

●

●

●

●

‒

●

●

Load1000

‒

‒

‒

‒

●

‒

●

●

●

Temp90

‒

‒

●

●

●

‒

●

‒

●

Temp110

‒

‒

●

●

‒

‒

‒

●

‒

Temp120

‒

‒

●

●

●

‒

●

‒

‒

Temp200

●

‒

‒

●

‒

‒

‒

‒

‒

Speed2.6

‒

●

●

●

‒

‒

●

‒

‒

Vib3

‒

‒

●

●

●

‒

●

●

‒

FOOD2

‒

‒

●

●

‒

●

●

‒

‒

CLEAN M

‒

●

●

●

‒

‒

‒

‒

‒

Motion2

‒

●

●

●

●

●

●

●

‒

  1. Other containers are available by agreement.

© Schaeffler Group USA